Use the following commands:
• MMEMory:DATA[:DEFinite] <"filename">, <data> - This command copies a file to the file system of the instrument. The filename should be the full path and filename. The query returns the contents of the specified file.
• MMEMory:EXPort:DLOG <"filename"> - This command exports the data that is currently loaded in the instrument's datalog viewer to a file. The export filename should be the full path and filename. The exported data is in .csv (comma separated values) format .
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |